SKINTOP® HYGIENIC

Stainless steel cable gland for use in the food and beverage industry

The new stainless steel Pintop® HYGIENIC cable gland is suitable for direct contact with food in production. Its suitability for use in food production is confirmed by certificates from ECOLAB®, and the design of the structure that meets EHEDG requirements.

Three key characteristics that make sure that SKINTOP® HYGIENIC can be easily cleaned and that allow it to be used in accordance with the strictest sanitary and hygienic standards: shape, precision of fit and material of manufacture. The rounded shape without edges and corners, the precision of fitting with a very low tolerance in production means that dirt has nowhere to accumulate. The material used for the production of SKINTOP® HYGIENIC is stainless steel of class V4A (1.4404), all this guarantees long-term resistance to difficult environmental conditions. Food-safe insulating materials are also used. A special elastomer, which is used for insulation, guarantees an extremely high degree of load reduction when the cable is stretched.

SKINTOP® HYGIENIC cable glands are available in sizes M 16 x 1.5 and M 20 x 1.5 since January 2015.

Your benefits with SKINTOP® HYGIENIC:

Suitable for direct contact with food
Certified by ECOLAB®
Easy to clean
It can be used with strict hygienic standards
Does not accumulate dirt


Many other Lapp branded products have been awarded an ECOLAB® certificate confirming their suitability for use in sensitive areas such as food and beverage production. For example, SILVYN® FG NM is a polymer protective sleeve that is safe for food. Thanks to its smooth surface, it is easy to clean, at the same time it prevents microbial contamination. ECOLAB® has also certified the SKINTOP® stainless steel cable entry, and bestsellers such as ÖLFLEX® CLASSIC 110 and other control cables, several UNITRONIC® data cables, ETHERLINE® network cables and FLEXIMARK® marking systems.

The SKINTOP® HYGIENIC stainless steel cable gland has been specially designed for use in the food and beverage industry

The SKINTOP® HYGIENIC stainless steel cable gland has been specially designed for use in the food and beverage industry